AXIS#.IL.COMPTABLE.MODULOVALUE

Description

The cogging compensation/torque compensation table has a built in modulo that can be used independently of general position feedback modulo. This modulo is performed on the input to the table (assuming the range is from 0 to AXIS#.IL.COMPTABLE.MODULOVALUE).

This defines the modulo position (starting from 0) that the input will wrap back to the first table entry. If using modulo, this value should generally be the same as AXIS#.IL.COMPTABLE.MAX.

Example

To set the modulo value of the table to 360 degrees, the user would enter:

-->AXIS1.IL.COMPTABLE.MODULOVALUE 360

Versions

Action Version Notes
Implemented 02-07-03-000

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

Linear: counts, mm, µm, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

360.0 Degrees

Data Type

Float
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
AXIS1.IL.COMPTABLE.MODULOVALUE

500ah

1dh

Signed32

Position

-

Read/Write

No

AXIS2.IL.COMPTABLE.MODULOVALUE

510ah

1dh

Signed32

Position

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IL.COMPTABLE.MODULOVALUE

5842

16D2

Signed32

Read/Write

Position

AXIS2.IL.COMPTABLE.MODULOVALUE

71378

116D

Signed32

Read/Write

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.COMPTABLE.MODULOVALUE

5842

Signed32

Read/Write

Position